8/23/2016 11:25 AM | |
Posts: 87 Rating: (0) |
This is to the end. |
8/23/2016 11:46 AM | |
Posts: 87 Rating: (0) |
I changed the cable and it was the same.Yes I downloaded, but simotion is not reachable. |
8/23/2016 12:04 PM | |
Posts: 87 Rating: (0) |
24VDC is connected, All leds are yellow. About number,, two times blinking 3 then two times 8 , and it is always like that. |