2/16/2017 4:52 AM | |
Joined: 5/12/2006 Last visit: 4/24/2024 Posts: 22226 Rating: (2980)
|
Hello, Jeff is right. Scout TIA doesn't support older SIMOTION D Devices, you can read this in the Product notification: OUT TIA V4.4 HF2 configures the SIMOTION C240/C240 PN motion controller as well as the SIMOTION D410-2 and D4x5-2 Control Units, including CX32-2/CBE30-2, in the TIA Portal with kernel/firmware version V4.3 and V4.4. In particular, the current version of SIMOTION SCOUT TIA V4.4 HF2 doesnotsupport the following SCOUT and TIA Portal functionality:
https://support.industry.siemens.com/cs/de/en/view/96311883 Regards |
2/17/2017 6:26 AM | |
Joined: 5/12/2006 Last visit: 4/24/2024 Posts: 22226 Rating: (2980)
|
Hello, which Scout Version do you use and from which Version you change the Simotion D to V4.4? Christoph |
10/20/2023 7:59 PM | |
Joined: 5/8/2022 Last visit: 11/22/2023 Posts: 1 Rating: (0) |
i have got the same problem. Maybe We should create the project from the beginning |
Follow us on