4/27/2018 9:51 AM | |
Posts: 64 Rating: (2) |
The antivirus is McAfee:
McAfee VirusScan Enterprise + AntiSpyware Enterprise: v8.8.0.1906 |
2/6/2019 11:26 AM | |
Joined: 1/10/2008 Last visit: 8/28/2023 Posts: 5 Rating: (1) |
I've had the same problem, also with Scout TIA V5.1 and V5.2 on the same computer running 'Sophos Endpoint Security and Control V10.8' on Win7 Professional. From Siemens support I've got the recommendation to use a special virus scanner from TrendMicro: https://support.industry.siemens.com/cs/ww/de/view/109743477 From Siemens support I've also got the hint to exclude the 'Siemens Scout process(es)' from on-access-scan if I want to continue using Sophos. This worked for me: I've excluded the process 'u7wwbfax.exe' for the Classic Scout versions and 'u7wpefax.exe' for the TIA Scouts. I didn't specify a path so the exclusions work for all processes with these names in any directory... Maybe this explanation can help anyone |
This contribution was helpful to2 thankful Users |