3/24/2013 9:30 AM | |
Joined: 1/16/2012 Last visit: 4/9/2021 Posts: 62 Rating:
|
Dear Experts, Your help is required, regarding the SIMOTION software. Our plant is equipped with several micromaster & sinamic drives and we have uploaded (in 2012) the all drives parameter backups on laptop through Driver ES - Starter V 4.2 Software.
All drives backup which we have on the CD and the all backups which we have uploded from drives are exactly the same, except one. When I open this parameter backup file from CD into STARTER software I received the following Info message: Software pacakage missing SoftwarePackage Type ID / VersionInfo There is some DCC chart alsoavailable in this backup, when I open it I received following Error: "The DCC chart cannot be opened" No valid license was found When I open the HW configuration I received the following: The project contains object of the software package 'SIMOTION', which cannot be edited because the software package is not installed or exist in an earlier version' Clicking OK, I received another message: Module which cannot be displaed with the installed STEP 7 version: HW Update Name Order No. Firmware Optional Package WinLC V1.x 6AU1 435-0AA00-0AA1 V4.1 SIMOTION
What will be the drawbback if I upload the drives parameter without these optional packages, If nothing then what is the benifits of these optional packages. Thanks & Best Reagrds AttachmentAttachment.zip (643 Downloads) |
3/1/2017 11:43 AM | |
Posts: 1529 Rating:
|
I REALLY hope that you made a backup before you attempt any of this. |
Follow us on