4/10/2019 4:18 PM | |
Posts: 1283 Rating:
|
I0.0 is a physical input whereas M0.0 is a memory area within the PLC and can be used in HMI to command this memory bit without use of physical connection. |
4/10/2019 4:25 PM | |
Posts: 2826 Rating:
|
Search for the PLC manual: (link) Focus on the chapter: (especially 5.2) Look at the video series: Navigate to the S7-archtecture video when you have entered through the portal (press the "play" button). |
Last edited by: #dP at: 4/10/2019 4:27:57 PMAdd link to manual |
|
4/10/2019 6:12 PM | |
Joined: 9/21/2012 Last visit: 10/2/2025 Posts: 4728 Rating:
|
Take some screenshots of your code, and add as attachment to here. It's easier to see whats wrong in your code. |
4/10/2019 6:59 PM | |
Posts: 45 Rating:
|
My project is 6 networks. These are the first 3. |
4/10/2019 7:00 PM | |
Posts: 45 Rating:
|
This is the second half of the project. |
Follow us on