6/3/2021 11:53 AM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1419)
|
As from TIA V17 there is a new feature: VoT (View of Things).In the United VoT for PLC web application the data that you have configured for a PLC in TIA Portal with Unified WinCC are displayed in a web browser. There is a detailed information about how to do it in the TIA help system (search for VoT and select the first item, “Configuring Unified VoT for PLC (RT Unified)” – It is also available in the navigation Information System, Visualizing Process with View of Things (RT Unified)) Here there are the main steps:
TIPs:
Sample project AttachmentUni2_20210603_0649.zip (1321 Downloads) |
Last edited by: Denilson Pegaia at: 06/03/2021 11:54:33Last edited by: Denilson Pegaia at: 06/18/2021 22:15:22Last edited by: Denilson Pegaia at: 06/19/2021 14:19:35Last edited by: Denilson Pegaia at: 12/22/2021 10:53:05TIP to fix bugs in TIA V17 up2 Last edited by: Denilson Pegaia at: 02/04/2022 10:55:53Denilson Pegaia |
|
This contribution was helpful to10 thankful Users |
2/3/2022 10:08 AM | |
Joined: 10/16/2007 Last visit: 4/19/2024 Posts: 11 Rating: (0) |
Hello Denilson Which is the workaround to run VoT with TIA V17Upd 2? The attached FAQ link https://support.industry.siemens.com/cs/ww/en/view/109804791 go to "Download Hotfix 9 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SR2" Thanks for your help Regards Jose |
2/4/2022 10:56 AM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1419)
|
Hi, sorry for the mistake, the right link is https://support.industry.siemens.com/cs/br/en/view/1098054633 |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on