Industry Online Support
Technical Forum
4/17/2012 2:20 PM | |
Posts: 30 Rating: (1) |
Though I am also beginner I finally managed after a lot of fighting to create simple and straight forward project that everyone woul understand. So I want to share my experience with other beginners... Project can be downloaded over here, just follow middle section without registering, only rewrite some strange characters.... http://uloz.to/xUy7idX/pidregulator-demo-wincc-rar The project is running on SINGLE computer, it consists of: - library PID regulator excited with either 100 or 20 value on its input, command arrives from WinCC application pushbutton, it is called every one second in OB32 - start PLCSIM with TCP/IP protocol a download software to it from simatic manager - start WinCC project (zzz) , by pressing pushbutton you can see different required value and response from PID regulator This design is completely minimalistic so very simple to understand! I believe it is always better to go step-by-step not to read 1000 pages manuals..... :-) |
This contribution was helpful to1 thankful Users |
4/21/2012 1:14 PM | |
Joined: 8/18/2009 Last visit: 2/22/2024 Posts: 541 Rating: (33) |
thanks sky59... Please tell me sample PLC +wincc projectfor Redundant CPU, I/O .....so that I can understand....
|
Last edited by: RAJKIRAN at: 4/21/2012 1:15 PMRajkiran Patil |
|
6/2/2014 9:52 AM | |
Posts: 1 Rating: (0) |
thanks for sharing your experience, can you please share it another host please, and there is lot things to ask about PID Regulator. |