7/26/2019 5:24 PM | |
Joined: 12/29/2011 Last visit: 1/1/2024 Posts: 20 Rating: (0) |
Running PLC 1215 with Basic HMI KTP 700 connected via IP-Switch. With some projects kan start olso simulated HMI and 2 HMI communicate with PLC, but in others projects simulated HMI does not communicate with PLC. Why? ------------------------------------------------------------------------------------------ |
Last edited by: AlexSen at: 07/26/2019 17:30:47Last edited by: Jen_Moderator at: 07/29/2019 05:50:38New subject after splitting |
|
7/29/2019 12:47 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello check this out: https://support.industry.siemens.com/cs/ww/en/view/88193789 And also check if you have selected the newest Image for the Panel in the TIA Portal Project. Bye Murof |
If this Information really helps, you could use the Rate function |
|
8/4/2019 4:34 AM | |
Posts: 12 Rating: (0) |
Hi, Does the Running simulation and real HMI are communicating to the same PLC ? If Yes -> each PLC has a specific limit of connection with the HMI Regards, Neren |
Follow us on