7/27/2015 8:02 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Please set the correct MODE for the input signal type... See attached file which I got from the helpfile (please check the helpfile for more modes). Normally the MODE parameter is automatically connected to the input signal when generating module drivers. You can also set the MODE yourself. Let me know if it is the solution. Grtzz |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on