8/28/2018 9:17 AM | |
Joined: 4/8/2016 Last visit: 2/13/2024 Posts: 133 Rating: (45) |
Hey RajaVijay, do you have a SIMIT Unit or do you use the virtual controller? If you use the virtual controller you can create channel faults of analog values by manipulating the value so that it is out of range. Simulating channel faults of digital values is currently only possible with a little workaround. With workaround I mean you can simulate a channel fault of a digital input by manipulating the Mode_xx input of the corresponding module driver. See the attachment for further information. If you have a SIMIT Unit and SIMIT V10.0 you can create device and module and channel faults as described in the manual, see chapter 2.5.6.7 https://support.industry.siemens.com/cs/ww/en/view/109759317 |
Last edited by: 51N3P at: 8/29/2018 9:47:16 AMKind regards |
|
Follow us on