2/26/2021 7:41 AM | |
Joined: 4/23/2010 Last visit: 4/11/2021 Posts: 6548 Rating:
|
Hello, If only motor speed is to be measure, no critical referencing required & if encoder cable interfacing length is more (more than 100 m), then you can select incremental HTL encoder with 10 to 30 V DC supply. Depending upon mounting requirement you may select syncho flange or clamp flange & select type of connection you need. Please refer attached sheet, which shall help you to order desired encoder. AttachmentRotary encoder data sheet.pdf (8 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on