Industry Online Support
Technical Forum
9/19/2013 8:17 PM | |||||||||
Posts: 767 Rating: (69) |
Hello edsel lin, For the SINAMICS G120 modular architecture style to achieve this type of functionality, the CU250S-2 controller will need to be used with the power module according to the motor current needs of the application. The CU250S-2 provides the interface for feedback from incremental encoder for closed loop speed control. Below are specific part numbers for the CU250S-2 controller according to specific communication needs for application.
Below is operating instructions. SINAMICS G120 Converter with the CU250S-2 Control Unit (vector) https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=78794884&nodeid0=36426537&nodeid1=24462795&nodeid2=11774653&onlyConfigurable=on&ehbid=html_76%2Fehb%2F78794884%2Ehtm&nodeid=78794927&load=content&csQuery0=CU250S%2D2&subtype=130000&lang=en&extranet=standard&viewreg=WW&u=NDAwMDAxNwAA&siteID=cseus Best Regards, Deputy |
||||||||
Follow us on