8/6/2012 8:38 PM | |
Joined: 4/21/2006 Last visit: 9/23/2024 Posts: 510 Rating: (24) |
Here you can find another interesting thread to this issue: FbDrive block in V8.0 update1. |
4/5/2016 9:51 AM | |
Joined: 6/23/2008 Last visit: 9/25/2024 Posts: 1168 Rating: (282)
|
Hello G_R_E_Y
Wich library you mean? The library Drive ES PCS7 Vx.y or do you mean the block FbDrive? The block FBDrive is included in PCS7 from version 8.0. This block supports the Standard Telegrams 1 and 20. This block works also with non Siemens drives, as long they support the telegram 1 or 20. As you are on V6.1 it's no option for you. The library Drive ES PCS7 Vx.y was also available for your version (6.1). If you could still purchase it, you need to figure out with the Siemens Sales Department responsible for your region. This library is only for Siemens drives. It works
with the Siemens telegram 352. This is the same like the Standard
Telegram 20 plus a warning number and fault number attached to the
telegram. The library comes also with a textlibrary, so the warning or
fault will be shown in clear text in runtime of the OS.
If you want to know the differences between the different telegrams and how the telegrams are build up in detail, have a look into the List Manual of your inverter. I will give you an example here for G120 with CU240B/E-2: Link You will find the relevant information in chapter 2.6. The interesting part starts at page 2-551. Best regards.. P.S.: Both, the FbDrive and the library Drive ES PCS7, supports the driver wizard of PCS7. |
Last edited by: mark1507 at: 4/5/2016 10:06:52 AM"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
This contribution was helpful to2 thankful Users |
4/5/2016 9:53 AM | |
Joined: 9/16/2013 Last visit: 9/18/2024 Posts: 199 Rating: (23) |
Hej, I'm not a PCS7 User, but if you don't want to use this library, you could communicate with the G120 like a normal Step7 CPU communicates: https://support.industry.siemens.com/cs/de/en/view/38844967 |
Last edited by: Gordon Shumway at: 4/5/2016 9:55:00 AM |
|
This contribution was helpful to2 thankful Users |
4/5/2016 12:11 PM | |
Joined: 5/26/2011 Last visit: 8/5/2024 Posts: 456 Rating: (7) |
I see. That's quite some read hehe. I'm yet to check the specific device, but I also found a very simple instruction without using additionally purchased libraries, which uses "Standard Telegram 1" which seems just 4 words: I hope I could use this to the actual device hehe. But still there seems to be no specific description of what exactly are those 4 words? Thanks! |
Last edited by: Min_Moderator at: 4/5/2016 12:56:38 PMEdit link to permanent one |
|
4/5/2016 12:14 PM | |
Joined: 5/26/2011 Last visit: 8/5/2024 Posts: 456 Rating: (7) |
That could really be helpful, but unfortunately we'll be using Profibus DP (it will be added to the last node of the CPU400 Master DP CP). I haven't checked it thoroughly though, maybe there's also things that could help me. Thanks! |
Follow us on