4/21/2016 11:27 AM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
The message frame 352 is only modifiable if you use the Drive ES block. When using the APL standard solution, the frame is not modifiable or extendable. You can check out the following manual: Configuration with Sinamics and DriveES chapter 6.1 explains the hardware configuration. |
Last edited by: Oreca at: 4/21/2016 11:31:03 AMIf I could help you, you can use the RATE button. Thank you. |
|
4/22/2016 7:46 AM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Hello RaviS, Sorry for the late reply. I think you are in the wrong screen. I currently don't have access to my DriveES software, but you have to check the slave properties itself in order to change the message frame. Not the individual words/modules. See attachment... I hope this helps you! |
If I could help you, you can use the RATE button. Thank you. |
|
4/25/2016 1:03 PM |
|
Joined: 6/11/2007 Last visit: 5/31/2024 Posts: 61 Rating: (6) |
Hello Anybody faced above problem and has solution for it. Kindly help Ravi |
Thanks |
|
4/25/2016 1:33 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Hi Autoguy, When DriveEs is installed, the DriveES profile is available in hardware catalog. When you use this profile (selecting modules under this profile), you will receive additional settings especially made for your drives. An overview is attached. When you don't use this profile, some functionality as attached is not available. Are you using the DriveES profile? If not, I suggest you use this and I think you will receive additional functionality. I hope I could help you with this as much as possible! That is all I know Best regards! |
Last edited by: Oreca at: 4/25/2016 1:36:12 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/28/2016 11:57 AM |
|
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Hi Ravi123@, What's your status? Did you solve your issue? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on