9/7/2016 5:55 PM | |
Posts: 1529 Rating: (202) |
Are you in Vector Control? If so, this is normal. The drive is providing flux current, which is about 30% of full nameplate current. No worries about this. |
9/9/2016 7:34 PM | |
Posts: 32 Rating: (0) |
@ apesky- I am running two VSD in Parallel to run the common motor. I have read the current in r068 parameter- Absolute current actual value. The same current that we read in parameter is the current by measuring by Clamp meter. There is no such heat rise on motor. I have attached one trace file- Which will give more details- Please suggest further- Attachmenttrace (1).docx (277 Downloads) |
9/11/2016 1:53 PM | |
Posts: 32 Rating: (0) |
|
Follow us on