11/21/2017 7:10 PM | |
Joined: 5/31/2012 Last visit: 1/4/2024 Posts: 23 Rating: (0) |
Dear Expert i have Simotion D435 program when i try to open with scout V4.1 it ask to converted because this program is programmed with V3.2 the problem is after i download this converted problem to D435 i get SINAMICS_Integrated offline where the connection to CPU is good note : i use PROFIBUS TO connect PG to D435 so what is the problem AttachmentS53292d0.zip (33 Downloads) |
Follow us on