2/1/2019 10:21 AM | |
Joined: 12/18/2018 Last visit: 5/29/2024 Posts: 27 Rating: (0) |
Dear Sirs Thank you for your support To compare the data and the alarm list of same equipment we connected to the control unit SINAMICS S120 CU320-2 DP V4.6 and downloaded the data to the PC. Regarding fault code 30015 in the alarm list, we checked the connection of cables to the power unit, junction box, terminal box of an induction motor. The insulation resistance of the cable and the asynchronous motor was tested. A07496 – please help how to solve that issue Was Compared parameters between same machines pilot gas valve . Differences in the parameter P2525. is it affect to normal operating CU? (see attached pic) This problem has existed since the machine was commissioned. attached zip file includs starter sinamics project files, screenshots of alarmlist, difference B&C machine pilot gas valve parameters Best regards Allashov Batyrbek
Attachmentgt.zip (196 Downloads) |
Last edited by: batyan at: 2/12/2019 4:24:46 AMLast edited by: batyan at: 2/12/2019 4:31:02 AM |
|
This contribution was helpful to1 thankful Users |
2/11/2019 4:15 AM | |
Joined: 12/18/2018 Last visit: 5/29/2024 Posts: 27 Rating: (0) |
Hello control unit SINAMICS S120 CU320-2 DP V4.6 |
2/14/2019 5:10 AM | |
Joined: 12/18/2018 Last visit: 5/29/2024 Posts: 27 Rating: (0) |
Hello Thank you for support Into the Attached Zip file included screenshots, project files starter with Best regards Attachmentgt.zip (162 Downloads) |
2/19/2019 4:12 AM | |
Joined: 12/18/2018 Last visit: 5/29/2024 Posts: 27 Rating: (0) |
no any idea and question? |
8/1/2019 7:45 AM | |
Joined: 12/18/2018 Last visit: 5/29/2024 Posts: 27 Rating: (0) |
dear Sir see attached zip Attachmentgtgpilot.zip (145 Downloads) |
Follow us on