6/17/2016 1:38 AM | |
Joined: 12/16/2011 Last visit: 5/17/2022 Posts: 26 Rating: (0) |
Dc link Sinamics S120 CU320 while is running normally the dc link instantaneous tripped and i get the faults below F30851; F34885; F01800; F30897; F34897 Anybody knows the reason , what is going wrong? I have already change TM31 and all drive Cliq cables and the problem still stand. Thanks in advance
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/17/2016 10:05:17 AMNew subject after splitting |
|
6/19/2016 11:17 AM | |
Joined: 12/16/2011 Last visit: 5/17/2022 Posts: 26 Rating: (0) |
It is old running machine (multidrive smart line module) My trouble on dc link only not in motor or encoder. |
6/19/2016 12:54 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Yes I understand. Please check the values in r0949 & in r2124 - [0] to [5] & report here. |
6/29/2016 11:51 AM | |
Joined: 12/16/2011 Last visit: 5/17/2022 Posts: 26 Rating: (0) |
Dear/sir kindly find the attached backup for DRM01 -DC LINK ,during trouble please check it note: my trouble in dc link. AttachmentDRM01.zip (641 Downloads) |
7/11/2016 9:56 PM | |
Joined: 12/16/2011 Last visit: 5/17/2022 Posts: 26 Rating: (0) |
Any update please |
7/22/2017 7:59 PM | |
Joined: 7/10/2015 Last visit: 6/15/2022 Posts: 2 Rating: (0) |
We detected a problem with the CIB. |
This contribution was helpful to1 thankful Users |
Follow us on