6/27/2007 11:46 AM | |
Joined: 6/18/2007 Last visit: 7/3/2024 Posts: 6 Rating: (0) |
OK so if i will not use this terminal i have to leave it without connection or i have to connect 24VDC on it? |
6/28/2007 10:48 PM | |
Posts: 133 Rating: (13) |
Do not wire anything to EP terminals 3 and 4 on the motor module if you are not using Safe Integrated. |
7/2/2007 5:24 AM | |
Posts: 4 Rating: (0) |
https://support.automation.siemens.com/WW/llisapi.dll/csfetch/22099400/MC-FE-I-003-V11-EN.pdf?func=cslib.csFetch&nodeid=22168913 This document give me a lot of help. And if you don't want anything setup for Safety just don't wire anything into the terminals on Power unit, that is the EP24V+ and EPM. |