3/26/2017 2:55 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Maybe the number of encoder lines are not correct in the plc Also reference speed should be okay |
3/28/2017 6:09 AM | |
Joined: 3/25/2015 Last visit: 1/31/2024 Posts: 39 Rating: (0) |
Hi, Thank You for reply,i am not using additional encoder,i have sinamics v90 servo amplifier,servomotor. i have doubt in my mechanical ratio Gearbox 5:1 Pulley 29 teeth Belt 238 teeth Pulley Diameter 184.62mm Belt Length:2460 What is the gear ratio i have to enter in my v assistant drive Regards shanthakumar Attachmentgear ratio.doc (312 Downloads) |
4/1/2017 4:23 AM | |
Posts: 1529 Rating: (202) |
As explained earlier, your pulley diameter is the ratio of the diameter of the pulley that your motor is connected to and the pulley which is turning whatever is supposed to turn. You do know that a belt is attached to 2 pulleys, right? And please do not repost identical questions. https://support.industry.siemens.com/tf/ww/en/posts/mechanical-gear-ratio/164114/?page=0&pageSize=10 |
4/1/2017 6:06 AM | |
Joined: 3/25/2015 Last visit: 1/31/2024 Posts: 39 Rating: (0) |
Hi, Thankyou for your reply,sorry for posting identical issues,is there any error create fraction of decimals.foe example my ratio is 5*8.20689655=41.0344828 Regards shanthakumar Attachmentgear ratio.doc (250 Downloads) |
Last edited by: AutoGen_410769 at: 4/1/2017 6:10:18 AM |
|
4/3/2017 12:48 PM | |
Posts: 1529 Rating: (202) |
Could you post a diagram of your entire mechanical transmission system? The number of teeth in your belt is not relevant!!!!!!!!!!!!!!!!!!!!!!!!!!! |
Follow us on