5/24/2013 6:15 AM | |
Posts: 40 Rating: (0) |
Hey amit... From what you are giving ON command to V20...Is there any PLC communicating with V20...or the ON command is from hardwired digital inputs?
|
5/24/2013 2:12 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello, there are only a couple of timers in the free function blocks. The best way for your application would be a solution with a S7 1200 and USS protocoll. See also: http://support.automation.siemens.com/WW/view/en/63696870 An alternative would be the Cn004 connection macro 4 for 16 speeds via terminals and controling theterminals 8 to 11 binaryvia a plc or logo (if the logos timer are enough). |
With best regards, |
|
Follow us on