8/7/2019 3:41 PM | |
Joined: 10/11/2006 Last visit: 5/7/2024 Posts: 5834 Rating: (790)
|
Hello, it is the performance at motor shaft in S1 operation. nominal torque of 1.27Nm, 3000 RPM, 0.4kW power With S6 operation a higher torque is possible. Therefore rated current of the motor is higher. Rated current of motor (3phase) is 2,6 A. P= root 3 * 2,6A * 200V = 900 W So V90 must supply this value.
Please see torque diagram of motor in D33 catalog. Chapter 3/6 https://support.industry.siemens.com/cs/ww/en/view/109758233 |
With best regards, |
|
Follow us on