7/1/2008 8:06 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, To be able to control the device directly via AT commands, use a terminal program, e.g. HyperTerminal. Note the following settings: Make the connection: COM port to which the device is connected Speed: 19200 Bit/s Data bits: 8 Parity: NoStop bits: 1 Duplex: FullI would also check if your cable has the correct pinning. See the picture in annex from the manual: AttachmentMD720-Modem cable.zip (184 Downloads) |
Best regards |
|
7/2/2008 8:28 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Hello, You must use standard modem cable for that which has all 9 pins used. |
Best regards, |
|
7/2/2008 9:30 AM | |
Posts: 3 Rating: (0) |
Thanks to everyone. We've solved the problem. It was actually cable related. |
Follow us on