1/15/2020 2:11 PM | |
Joined: 1/6/2019 Last visit: 8/27/2022 Posts: 13 Rating: (0) |
Dear Dchartier, I am using LINXCOM UK ( 100M Multi Mode 550 M 850 nm ST To Single Mode 20 KM 1310 nm SC external power) converter. OLM1 : - SYSTEM : lit green - CH1 : lit yellow -CH2 : lit red -CH3: lit red -CH2-LEVEL : lit red -CH3-LEVEL : lit red OLM2 - SYSTEM : lit green - CH1 : lit yellow -CH2 : lit red -CH3: lit red -CH2-LEVEL : lit red -CH3-LEVEL : lit red Converter 1 : PWR : lit green LINK A : not lit LINK B: not lit Converter 2 : PWR : lit green LINK A : not lit LINK B: not lit I think i am confused with converters wiring , so can someone help me to connect two converters , and each converter to OLM Thank you Attachmentsinglemode-to-multimode-fibre-media-converters.pdf (77 Downloads) |
1/15/2020 4:25 PM | |
Joined: 1/6/2019 Last visit: 8/27/2022 Posts: 13 Rating: (0) |
Dear Duris, As you see in pictures: Tx (OLM1 ch3) --> Rx ( converter 1) Rx ( OLM1 ch3) --> Tx ( Converter 1) Tx ( converter 1) --> Rx ( converter 2) Rx ( conv 1) -->( Tx converter 2) Tx (OLM2 ch2) --> Rx ( converter 2) Rx ( OLM2 ch2) --> Tx ( Converter 2) Leds: OLM1 : - SYSTEM : lit green - CH1 : lit yellow -CH2 : lit red -CH3: lit red -CH2-LEVEL : lit red -CH3-LEVEL : lit green OLM2 - SYSTEM : lit green - CH1 : dosen't lit -CH2 : lit red -CH3: lit red -CH2-LEVEL : lit green -CH3-LEVEL : lit red What should i do to get communication in both channels please? AttachmentSM.zip (67 Downloads) |
1/16/2020 9:58 AM | |
Joined: 1/6/2019 Last visit: 8/27/2022 Posts: 13 Rating: (0) |
Dear Duris, i think i am connecting converter correctly, since i connect Send port of OLM to Rx of converter And receive port of OLM to Tx of converter Attached pictures , the wire with 0 is connected in Tx olm and Rx converter. Attachment15-01-2019.zip (61 Downloads) |
Follow us on