4/14/2021 2:17 PM | |
Joined: 2/7/2020 Last visit: 1/10/2024 Posts: 101 Rating: (0) |
Hello Ralfinio, First of all, Thank you for response. It was really good input. So, For Single station redundancy: 1. We configure 2 OS in project. These both OS runs individually. If one of OS fails, Data will get sync. Q: What do you exactly mean for "Data will get sync" because as project is same in both project, Data is also same in both OS. Or Sync means whatever parameters e.g. SP or commands will get transfer to Running stations. Please suggest.... 2. For this configuration, Is below licenses are good to buy? OS 6GK1162-3AA00 SIMATIC NET COMMUNICATION PROCESSOR CP 1623 PCI EXPRESS 6GK1716-0HB14-0AC0 SIMATIC NET, S7-REDCONNECT POWERPACK V14 6ES7652-3AA58-2YA0 SOFTWARE SIMATIC PCS 7 OS SINGLE STATION REDUNDANCY V9.0 (PO 100) 3. I will not able to connect client in this configuration. For Server redundancy: 1. For this configuration, Is below licenses are good to buy? 6GK1162-3AA00 SIMATIC NET COMMUNICATION PROCESSOR CP 1623 PCI EXPRESS 6GK1716-0HB14-0AC0 SIMATIC NET, S7-REDCONNECT POWERPACK V14 6ES76523BA582YA0 PCS 7 V9.0 OS Software Server Redundancy (100 PO) If any other licenses needed, Please suggest. Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/15/2021 11:27:22New subject after splitting |
|
4/15/2021 11:28 AM | |
Joined: 6/19/2017 Last visit: 5/8/2024 Posts: 8008 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Need input regarding Single station redundancy & server redundancy is published within the conference Process Control Systems SIMATIC PCS 7. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on