7/22/2013 11:45 AM | |
Posts: 11 Rating: (0) |
Thank you for your help! I have now changed the MD, can I save those values in R-parameters? how can I get the values in NC-part program? what i want to do is as follow: in synchronized action, when the spindle power achieve a certain value, the spindle will be stoped immediately. can you help me with some programing?
|
7/22/2013 12:46 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Which is your country? Please click contacts worldwide. This will help you to locate your nearest Siemens service support office. |
7/22/2013 1:08 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, If you want to ONLY check this, follow below mentioned proceduer. While spindle is in running condition, you can check spindle motor actual current value at MD 1719, say it is 30% I would suggest you to reduce value in spindle MD 1105 to lower rating, e.g. say from30 to 20. (MD1105 is reduction in maximum motor current) While running next cycle, when the actual current drawn by spindle motor is more than 20%, it will trip. By such trial & error method you may find out your desiered results. OR else, if you want to follow your method, please check this link. Hope this may help you. |
Last edited by: PISCEAN 2010 at: 7/22/2013 1:10 PMLast edited by: PISCEAN 2010 at: 7/22/2013 1:10 PMLink added |
|
8/5/2013 11:45 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
new question split to: Sinumerik 840 D - spindle power bar vizualisation. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|