Industry Online Support
Technical Forum
2/13/2012 7:31 AM | |
Posts: 2 Rating: (0) |
Hello, I have a big problem, my system is: Sinumerik: 6FC5 372-0AA00-0AA2 I have the toolbox 2.6 HF 4 but in the Hw config dont have this equipment, i have to use 6FC5 372-0AA00-0AA1, i hope that this not affect. The PLC works good but when the system try to recognize the drive system the telegram of CU is in red, Telegram 391, the version of ncu is and hardware are in the attachment. Please i need help because the ALM cant comunicate with ncu Attachmentversion.zip (83 Downloads) |
2/14/2012 1:12 AM | |
Posts: 2 Rating: (0) |
Hello! I have a PCU 50.3 with HMI Advanced and in the dont have alarm in the screen, the message appears when im reviewing the Profibus Link and i select the telegram 391 cause is in red. The message is as follows: Telegram configuration error p922=999 or p922<$MN_Drive_telegram_type or p922=0 or lenght of the $MN_drive_telegram_type slot > step7 slot lenght. I have the default configuration, the parameter p922 = 391 by default and i cant change that, if i try the options are 390, 391 and 392 The mcp is in healthy sign and the display is in 6. AttachmentNC.zip (73 Downloads) |
2/14/2012 11:15 AM | |
Posts: 63 Rating: (3) |
seems problem with HW conf of PLC project!!!????? |
Follow us on