11/8/2016 1:53 AM | |
Joined: 3/28/2010 Last visit: 9/18/2024 Posts: 1056 Rating: (213) |
LRV = 0.01 bar (is there some reason you don't use 0.0 bar for LRV?) URV = 1.00 bar The multilingual (multiple languages) Z-fold Quick Start Guide that is included with the DSII transmitter under one of the screw covers which Siemens calls a "Leporello" is at this link: Use Mode 6 to enter an exact value using the pushbuttons for the URV (Upper Range Value) |
Last edited by: The Helping Hand at: 11/8/2016 10:35:19 AMReplaced the temporary link against a permanent one. |
|
11/9/2016 5:48 AM | |
Posts: 67 Rating: (0) |
Thank you danw, by following your instruction its now okay. |
11/11/2016 3:55 AM | |
Posts: 67 Rating: (0) |
Thank you danw, Would you please explain with example. I am little bit confused about your speech. |
Follow us on