12/23/2019 5:17 PM | |
Joined: 1/6/2011 Last visit: 2/24/2024 Posts: 45 Rating: (0) |
Hi Siwarexi, [snip] But I have another SIWAREX which is still not working. Even after using 105 and 108 from SIWATOOL, TARE command is not working. Basically it is not even accepting the 105 and 108 commands and gives standstill not achieved. This happens even if standstill status is green in DR30. But the standstill status comes and goes. The weight shown in display also fluctuates so much and is not standstill, even if there is nothing on the load cell. I think there is some configuration error.Refer a screenshot I have attached. Also I have attached 3 FTA files. This is happening using all 3 FTA configuration files. Please suggest where I am going wrong? ------------------------------------------------------------------------------------------ AttachmentSIWAREX 421 problem.zip (436 Downloads) |
Last edited by: Jen_Moderator at: 12/25/2019 12:42:46New subject after splitting. Division of questions into seperate topics. |
|
Follow us on