1/27/2015 2:08 PM | |
Posts: 10 Rating: (1) |
Can you post a link to the device you wish to use, for more information please? Looking at theMAXREFDES36# (http://www.maximintegrated.com/en/design/reference-design-center/system-board/5879.html), it looks like you can use an additional power supply. However, you will have to insure that the slave is powered up be fore the Master sends the "Wake-Up" pulse to initiate communications with the slave. You will also have to map the IO yourself as the device is not in the catalog for IO-Link slaves in ES13. Respectfully, steven |
1/28/2015 9:17 AM | |
Posts: 11 Rating: (0) |
This is the module I am going to use http://www.balluff.com/balluff/MES/es/products/product_detail.jsp#/158187 Thank you Steven |
Follow us on