11/2/2015 11:23 AM | |
Joined: 8/3/2009 Last visit: 4/19/2024 Posts: 12816 Rating: (1634) |
Hi s_vb perhaps its a java Problem, then this Link could help you: https://support.industry.siemens.com/cs/ww/en/view/101977510 Look in the Taskbar of your Panel. is there on the right side a small icon like this: then the SmartServer is running. If not then go to Control Panel -> WinCC Internet Settings-> remote and start the Smart Server and control the start Settings. Try also the access with the Sm@rtClient application. This is installed also on your TIA Portal engeneering System or is on the Installatoin DVD of WinCC (Support/SmartClient) good luck Bye Murof |
Last edited by: The Helping Hand at: 11/2/2015 4:32:38 PMMade the link clickable If this Information really helps, you could use the Rate function |
|
Follow us on