Industry Online Support
Technical Forum
5/26/2012 9:59 PM | |
Posts: 25 Rating: (7) |
I found following information from Local Siemens Tech Support: It is not possible to use WebNavigator orSmart Access on an iOS or Android device. Both applications use an "exe" or require a "plug-in" to Internet Explorer. They suggested mebyimplementing someother Windows based solutionsby referring Web Navigator Compatibility matrix which list the allowed operating systems. http://support.automation.siemens.com/WW/view/en/26417216 Based on that I managed to shortlist few options available in the market which runs on Windows environment and which has WiFi connectivity. 1. Panasonic Toughbook CF-H1 OS:Windows 7 Computability: WebnavigatorAbove WinCC 7.0 SP2 Screen Size:10" (XGA) 2. Toshiba "JournE" OS:Windows CE 6.0 Computability: Above WinCC 6.0 Screen Size: 7" (TFT) Hope this will be useful. KD... |
10/1/2019 6:16 AM | |
Posts: 2 Rating: (0) |
That link does't work. |
Follow us on