12/10/2010 2:07 AM | |
Posts: 1 Rating: (0) |
i have a CPU FM 352-5 HIGH SPEED PROCESSOR MODULE. |
12/10/2010 4:35 AM | |
Posts: 510 Rating: (117)
|
Chapter 9 of the 352-5 module http://support.automation.siemens.com/WW/view/en/9240171, discusses using the module with non-S7 profibus masters. From the manual; " The non-S7 PLC must have DP Master capability and its configuration tool must be capable of importing the GSD file for the ET 200M. The FM 352-5 must have an MMC which has been programmed by STEP 7. The contents of the MMC must be SDB 32512 created in the STEP 7 environment as described in Chapters 5 and 6 of this manual. The user program of the non-S7 PLC must manage the data transfer between itself and the module according to the declared interface of the Application FB as programmed in STEP 7. It must also perform mode control via the control bytes." |