11/8/2010 2:31 PM | |
Joined: 4/20/2007 Last visit: 2/6/2024 Posts: 724 Rating: (42) |
See attachment. Thanks for taking your time to try to help me! Attachmenterror Step 7.pdf (324 Downloads) |
11/8/2010 10:27 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi Ton, Please look for the Hardware Support Package of this CP 343-1, it could be that this is not installed, so that only an older CP 343-1 (which one??) is installed in the hardware catalog of STEP7. You could read in this new version (when the STEP7 version can do something with it) in the hardware projecting. See also STEP 7 Hardware Support Packages (HSPs - as at 11/2010) for installing hardware updates in the Hardware Configuration It is also possible that the version of STEP7 is already updated some times with Service Packs.... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to1 thankful Users |
11/9/2010 10:24 AM | |
Joined: 4/20/2007 Last visit: 2/6/2024 Posts: 724 Rating: (42) |
Hi, It should be one of the newer modules. 343-1 advanced... Tried to install, got this picture... |
11/9/2010 12:27 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Ton, Seems you need some Hotfixs. Look at Simatic Manager nach Servicepack 5 Installation langsam beim Öffnen . But I can't remember which one from them was in SR6. Later I'll check and let you know. BR, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
11/10/2010 6:11 PM | |
Joined: 4/20/2007 Last visit: 2/6/2024 Posts: 724 Rating: (42) |
That did not help... Anyone any more options? |
Follow us on