1/18/2017 11:25 PM | |
Joined: 10/11/2014 Last visit: 5/27/2024 Posts: 79 Rating: (1) |
hi in software redundancy document it says : The IM 153-2 DP interface of ET 200M has two connections, i.e. one to the CPU in station A, and one to the CPU in station B. and in the example it uses im153-3 with two dp connection . but this product has been discontinued if we want to use im153-2 redundant with one connection what changes should be made . should we use two im153-2? is there any document or example? thank you |
Last edited by: Min_Moderator at: 1/19/2017 1:29:17 PMEdit link |
|
1/21/2017 9:58 PM | |
Joined: 10/11/2014 Last visit: 5/27/2024 Posts: 79 Rating: (1) |
is there any suggestion ? |
2/7/2017 4:20 AM | |
Joined: 4/25/2011 Last visit: 9/18/2024 Posts: 40 Rating: (1) |
Hello, It is not possible to make redundancy using one connection. You have to install two IM153-2 and one is connected to CPU-A and another is connected to CPU-B. Any Queries? |
Nobody is Perfect and i am nobody....If it is helpful please Rate it. |
|
This contribution was helpful to1 thankful Users |
Follow us on