4/18/2011 11:32 AM | |
Posts: 7 Rating: (0) |
Dear Sir, i am new to this software ws800a i have seven machine with 880 controller and i want to change my systems operating language from german to englsh ...can i do this work with ws800a software. i also want to purchase ws800a but not able to purchase ,,,can you tell me any place where i can purchase . apart from this all issue i have one question for this controller 880t .... i have one machine which is fitted with 880t ga2 software version 1.2... when i try to use this machines tool type 40 in tool offset table it shows error 2069 "5d wzlk nicht moeglish" and it is not working i want to use 5d machinning option on my machine my machine hase total 9 axis and i want to use automatic tool length conmensation when i rotate b axis in degree i want that tool pont is remain same position and rest of axis move according to this plane .... i never use this type of machinning in past ...my company is in india and we purchase machine from germany... thanks kalpesh patel Splitted from WS800A CNC 840C. |
Last edited by: O_Moderator at: 4/18/2011 11:52 AMnew subject after splitting |
|
5/6/2011 5:50 PM | |
Posts: 7 Rating: (0) |
Thank you very much for spend time i will do as you told me then if i face any problem i will tell you ... thanks |
5/12/2011 4:13 PM | |
Posts: 7 Rating: (0) |
Dear Pee El Sea I try to download cycle from my machine with following procedure go to >dignose>standard>status>plc status>db>48 input>then i can see on scree that cycle release bit number 11 is =1 then i set this db48 D0.11=0 and try to send l306 cycle from my machine to my pc via serial port -1 but after 3 second nothind happened and DIO disapear.... and withou pressing reset i again go to db48 and i can see that db48 D0.11=0 is there is further process for this procedure...... and i attached my machines sheet please look this we have3d opton as a standard and we only need to set ncmd to use 5 axis tool length correction. and as you told me now i understand we can change l306 cycle and use as subprogramm (is it ok what i am thinking can we use l306 cycle after correction as a normal subprogram file) and for 5d tool length correction i read in 840c manual that we can only run first five axis with tool type 40 ....and in 840c G15 is code with we can use this option ....and my machine has B1 axis which is sixth number .....other wise with tool type 40 i can use my first five axis without any error ...and when i try to run B1 axis it shows 2069 error ...may i can change axs number and check ...... and then i try to change axis but unable because it shows erroe ..... i have simple question for this 1-can i change my axis from nc md and can i make my first axis as a sixth axis and sixth axis as a first axis so i can check weather 5d tool length correction is working with my B1 axis or not. and thanks for your support and spend time for me...... Attachment3.zip (118 Downloads) |
Follow us on