1/14/2012 9:53 PM | |
Posts: 3 Rating: (0) |
Dear friends i would like your help. Does anyone know where can i find solar tracking function block for s7-1200? Thank you!! |
1/15/2012 12:34 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054) |
Hello Thodoris I don't think that the S7-1200 Solar tracking FB is availabel as a free download and suggest you get in touch with your local Siemens office to find out if so (or howyou'llneed to pay for it if it ispurchaseable). You'll find the general info about it including a brochure at THIS link. Having said that, the free of charge Step7 OSCAT library (see www.oscat.de) also contains a Solar tracking Algorithm which may be useful for your application. Since the Blocks are programmed in (Step7 V5.x) SCL, you'd need the lastest S7-1200 firmware and TIA Portal version(V11 SP2) and would have to convert the Block over to it, but it may be worth the effort. I hope this helps |
Cheers |
|
1/15/2012 11:51 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054) |
Hello Thodoris as mentioned in my previous post,the OSCAT library is developed in Step 7 V5.x format, you'll need to do a migration to TIA Portal Step 7 format firstand the link below has more on this: What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional V11? I hope this helps |
Cheers |
|
Follow us on