10/23/2018 7:48 AM | |
Joined: 4/28/2015 Last visit: 12/16/2019 Posts: 1221 Rating:
|
Hi, with static IP there is something additional to do. You have to set the gateway, which you have already done. The other thing is to add the DNS nameserver, because this is not automatically done when the interface is set to static IP. Then you have to make this file immutable because otherwise it will be overwritten with every boot. How do that is described here. I am wondering why it is not working with DHCP.. But try it with the DNS "fix" ;-) Best regards! |
This contribution was helpful to
1 thankful Users |
10/23/2018 8:17 AM | |
Joined: 6/25/2018 Last visit: 12/16/2019 Posts: 16 Rating:
|
Thanks Bergmanu, it works perfectly with this fix. |
This contribution was helpful to
1 thankful Users |
Follow us on