7/11/2018 4:22 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32882 Rating: (4065)
|
@NIBOU, everything is right and are also interesting information. He does not want to save a LOGO! Program on the SD card, but a LWE project. Edit: That his LOGO! detects that an SD card is plugged, can be recognized by the error message. Diagnostics |
Last edited by: ixo65 at: 7/11/2018 4:35:32 AM |
|
7/11/2018 8:01 AM | |
Posts: 2930 Rating: (432)
|
@erwan84, check Wikipedia (search: FAT32) and read the article. Here you get an explanaition what the problem is. For Linux and Mac there are different driver for formating cards. As you made (together with your friend) use windows PC to format the card (Win7: Fat32 Standard). However , if it still don't work, check: + if you plug in and remove the card switch LOGO! to STOP-Mode + Check if the MSD-card holder if it is pressed in is plan with the LOGO! housing. Some user press in the holder stronlgy and this may result in damadged pins on the holder inside. If this happen, then the holder is not plan with the LOGO! housing. + Insert the MSD.card right: If you look to the front of LOGO!, then the pins of the card must be on the top. Hope this helps |
Follow us on