12/2/2008 1:42 PM | |
Posts: 1776 Rating: (95)
|
Hi, for this AddOn contact to the e-mail in the FAQ http://support.automation.siemens.com/WW/view/de/9985721 or use the link for FAQs for the CPU Diagnostic tool http://www.industry.siemens.com/IT4Industry/EN/SOLUTION_SERVICES/SIMATIC_ADDONS/DIAG_DOWNLOAD.HTM |
12/2/2008 3:06 PM | |
Joined: 5/23/2008 Last visit: 9/29/2009 Posts: 10 Rating: (1) |
HARDWARE: CPU 416-2 for most of them, 416-3, 416F-2 FIRMWARE: V5.1.1 QCPU_STATE: i would like to do more tests and go further in the CPUSTATE variabe, but no time to do this today, sorry... only 3 cases on all my CPU's:
So my problem is with CPUSTATE= 16#71... Does this state mean that th CPU is INTF? if it is not the case the problem comes from S7 and in the other case from WinCC/System Diagnostics Really thank a lot for your helpWüstenräuber See U |
12/2/2008 3:33 PM | |
Joined: 10/3/2008 Last visit: 4/6/2024 Posts: 954 Rating: (123) |
I see in your screenshot that the information of the CPU aren't shown. In the white scree the MLFB, Hardware- and Firmwareversion should be shown (read out from CPU online). Please export the cfg-File from HW-config and parameterize it in the ocx again. You could also attach your cfg-file (of a 416-2 CPU) and I can test it as well. Wüstenräuber |
12/2/2008 4:33 PM | |
Joined: 5/23/2008 Last visit: 9/29/2009 Posts: 10 Rating: (1) |
i feel really stupid... The licence were not correctly installed on the server. just after i installed them with the yellow floppy disk, all was correct! Shame on me... Sorry for wasting your time
|
12/2/2008 8:59 PM | |
Joined: 10/3/2008 Last visit: 4/6/2024 Posts: 954 Rating: (123) |
Hi, great, that it's okay now! One question: If this was a license problem: Normally you should get an error message regarding the missing license.(?) Wüstenräuber |
12/8/2008 11:09 AM | |
Joined: 5/23/2008 Last visit: 9/29/2009 Posts: 10 Rating: (1) |
I get no error message on redundant server... Thank for all your help again...
|