Industry Online Support
Technical Forum
3/17/2009 3:24 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello Eastern; You could look at the following sorting program provided by Siemens: http://support.automation.siemens.com/WW/view/en/865058 Unfortunately, it sorts in descending order.... Just study the source files, you should be able to understand the underlying mechanisms in play. Either you can reverse the order of testing so you make a descending order, or you invert the resulting list after the program provides an output DB. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
3/17/2009 3:35 PM | |
Posts: 557 Rating: (64) |
Dear Sir, thank you very much for reply regards |
3/17/2009 4:06 PM | |
Posts: 22 Rating: (2) |
Hi There is some old: Find in standard Library - TI-S7 Converting Blocks Add to Table: FC84 As a feature the result is sort ascending |
3/17/2009 4:16 PM | |
Posts: 22 Rating: (2) |
Hi As another posibility you can try to seek at: boble sort, but take care of zero values. Attachmentfc1_e.zip (303 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on