Industry Online Support
Technical Forum
3/23/2010 3:03 AM | |
Posts: 29 Rating: (0) |
Hi... |
3/23/2010 9:16 AM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839)
|
Hello luciferC4, The answer is YES, you can use these inputs as standard inputs. CPU314IFM have 20 integrated digital inputs; 124.0 to 126.3 and of those are 4 inputs are for integrated functions (126.0 to 126.3) please see page 111 of the following manual. S7-300 Automation System, Hardware and Installation: CPU 312IFM - 318-2 DP Also you can use these inputs as standard inputs as well if you do not want to use them within the integrated function. Please look in page 154 of the following manual S7-300 Integrated Functions CPU 312 IFM/314 IFM Hope this helps, |
Last edited by: Ayman Elotaify at: 3/23/2010 9:17 AMcorrection of page numbers Ayman Elotaify |
|
Follow us on