7/9/2019 7:01 AM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (295) |
Hi, for the communication to the drive and for controlling it I would highly recommend to use one of those options: 1) use Technology Object 2) use the drive with standard telegram 1 and the Function Block "SINA_SPEED" from the DriveLib library, which is very simple to handle (just enabling the axis and giving a speed setpoint; as feedback you get the axis state and actual speed) - if Startdrive is installed to TIA you already have this lib installed, if not you can get it here: https://support.industry.siemens.com/cs/ww/en/view/109475044 |
Best regards, |
|
Follow us on