2/9/2009 8:35 AM | |
Posts: 33 Rating: (0) |
try to use configuration tool for excel ( i think, it is in options section, when installing wincc) it have sheets for tags, alarms and so on. |
2/9/2009 11:11 AM | |
Posts: 4 Rating: (0) |
i have the wincc tool on excell but it only imports the alarm logging, and do not export the excel file to the wincc. |
2/9/2009 2:02 PM | |
Posts: 33 Rating: (0) |
then try to do deeper rtfm :). this tool for sure does import data back to wincc. i use it all the time to create my tags alarms and archyves. |
2/9/2009 5:05 PM | |
Posts: 4 Rating: (0) |
sorry for my ignorance but i don't know what tool is that, and using that tool i can export from excel to wincc alarm logging? and add to the existing alarms? |
2/16/2009 11:36 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi, it Works fine in WInCC V6.2 SP2. I can import the alarms from Excel to WinCC use the function "write alarms" |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
2/16/2009 3:22 PM | |
Posts: 4 Rating: (0) |
hi, i got the wincc 6.2 but i haven't that tool. the only tool in excell that i have, is the import one. to import the project to wincc, alarms tags etc |
Follow us on