9/4/2008 7:24 AM | |
Posts: 38 Rating: (3) |
Hi all This is anirban here. I just tried to install a fresh copy of PCS7 v 7.0 into my laptop today. My laptop is a "Compaq 8510p" with Windows XP SP2 installed. I've done this insttaltion so many time before. But now whenever I am trying to install the SQL Server 2005 into my new laptop (nothing installed except the OS), the installer is behaving like a devil. It is going normally till the installer is trying to install "MSXML 6". At this time the installer is showning that the "Setup Failed" notification. Also a setup log file is being generated into the setup folder of the SQL Server. I gone through the log file but it is not possible for me to understand what is there in the log file. I am attaching the log file for your reference. Now anybody know what is the problem? If anybody is there to help me please help me... Regards Anirban AttachmentMSXML6_Log.pdf (415 Downloads) |
Last edited by: anirban at: 12/2/2008 12:09 PM |
|
9/4/2008 9:19 AM | |
Posts: 487 Rating: (36) |
Hi Could be privilege problem , must be admin to install ,try contacting microsoft and Siemens Eric |
9/4/2008 5:12 PM | |
Joined: 9/11/2006 Last visit: 3/17/2022 Posts: 168 Rating: (6) |
Hi anirban Are you able to install message queing(under windows components)without any problems |
9/5/2008 9:01 AM | |
Posts: 38 Rating: (3) |
Hi all AttachmentWin CUU.zip (929 Downloads) |
This contribution was helpful to6 thankful Users |
Follow us on