Industry Online Support
Technical Forum
6/5/2014 4:52 AM | |
Posts: 10 Rating: (1) |
Hi all I tried to install PCS7 with WinCC but this error came out as per attached. How to fix it? Thanks guys!
|
6/5/2014 9:18 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! For complete installation instructions please refer to atached document. However, I would like to ask, which operating system you are using? The following operating systems are supported in PCS 7 V8.0 incl. SP1 : ● Windows XP Embedded Standard 2009 ● Windows XP Professional SP3 (32Bit) ● Windows Server 2003 SP2 Standard Edition (32Bit) ● Windows Server 2003 R2 SP2 Standard Edition (32Bit) ● Windows 7 Ultimate/Enterprise SP1 (32Bit) ● Windows 7 Ultimate/Enterprise SP1 (64Bit) ● Windows Server 2008 SP2 Standard Edition (32Bit) ● Windows Server 2008 R2 SP1 Standard Edition (64 Bit) Also, in manual specified, when you update the software to PCS 7 V8.0 SP1, components of a previously installed SQL Server 2005 could be retained on the computer. These do not affect operation of PCS 7 V8.0 SP1 with SQL Server 2008 R2. Attachmentpcs7-readme_en-US.pdf (291 Downloads) |
Last edited by: olloy at: 6/5/2014 9:19 AMDear moderator, please move the topic to PCS7 conference. |
|
7/23/2014 8:43 AM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoinstall pcs 7 V8.0 with windows7 professional sp1 OS. With best regards, Narrator1
|
Follow us on