Industry Online Support
Technical Forum
8/10/2007 7:58 AM | |
Joined: 10/3/2006 Last visit: 1/5/2024 Posts: 44 Rating: (0) |
Hi, I would like to know which databases I should include when creating a backup of the Central Archive Server. I created a database maintenance plan of creating backups of all the databases every 12nn, twice a week. Most of the time, back-up is successful, but sometimes it is not. I have included a log file of the database maintenance plan from SQL as reference. According to the log file, it seems that I should not include all the databases. Do you have any technical documents regarding this? Regards, Jenie AttachmentDB Backup Failed Logs.zip (393 Downloads) |
Last edited by: jenie at: 10.08.2007 08:00 |
|
8/18/2007 8:56 AM | |
Joined: 8/10/2006 Last visit: 8/13/2024 Posts: 298 Rating: (29) |
My understanding is the databases configured are stored in SQL Server, and automatically managed. |