5/14/2014 6:39 PM | |
Posts: 2661 Rating: (279)
|
Hi n00dels, Run the OSPE and a complete OS compile with memory reset. Was this project created with PCS7 V8.0 SP1 Update 1 or with a version before Update 1? Also, can you provide screenshots of the faceplates? BTW, PCS7 V8.0 SP1 Update 1 contains WinCC V7.2 Update 5. I strongly recommend upgrading your WinCC V7.2 to Update 6: Update 6 for WinCC V7.2 and WinCC V7.2 ASIA Regards |
5/15/2014 2:09 PM | |
Joined: 4/8/2013 Last visit: 3/11/2024 Posts: 95 Rating: (7) |
I have already the latest version of WINCC installed with update 6. running the OSPE and a complete recompile with memory reset have no effect. i seriously think there is a problem with the VBS runtime somehow since the sameproblem does not occur on other stations i have attached a screenshot of the problem AttachmentC:\Users\z0032ewf\Desktop\Problem_VBS.zip (97 Downloads) |
5/15/2014 5:47 PM | |
Posts: 2661 Rating: (279)
|
If this is occurring only on one station then I would suspect the WinCC installation on that station... |
1/18/2015 9:27 PM | |
Posts: 28 Rating: (0) |
Hello Jules, I did run the OS project editor again and the same problem persists. I made a test project but also the same problem. Im clueless right now. |
Follow us on