7/1/2006 2:49 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
[quote user="hakangs"]At the side the scada computer is broken.The S5 scada computer is Simatic PCRI 45 .Do all the mentioned FB make communication between S5 CPU and Simatic Scada Software. Do I need them at my S7 converted program? If I must convert them how can I convert these bloks to S7 standart function ? If you use WinCC as Scada system then with other blocks it will work directly (also COM PMC), http://support.automation.siemens.com/WW/view/en/22302599have the newest software for this. But if you use another Scada system you need to replace all this blocks with 'equivalent' blocks of the Scada system. Normally other Scada systems doesn't have equivalent blocks... and use a send and receive off all data. There are then no accurate timestamps, the Scada is making the time stamps. [:(] PC RI45 doesn't say anything about the used Scada (that's only a industrial PC), if you use another PC then the software will work if there is a idea of the whole number, i maybe could find what software was installed and what you can do to solve this problem. [:P] The SIMATIC S5 PMCPRO manual you can download under the following link: http://support.automation.siemens.com/WW/view/en/19376392 Please consider what's used, normally PMC PRO made the PLC leading, if something is changed there is made a event (like S7 whit ALARM-blocks) and the Scada have only to get this information. [:o] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on