9/26/2013 9:38 PM | |
Joined: 10/3/2010 Last visit: 3/14/2024 Posts: 1552 Rating: (188) |
Had something similar not so long ago, in case you have clients without own project? If you open the project located on the server from your client PC, check first the share name of the project on your server. Make a shortcut on the clients desktop using \\servername\WinCCProjectName\WinCCProjectName.mcp Do not use the full network path to your mcp file. Off course the above is only for clients without project. |
B r g d s , |
|
9/27/2013 8:39 AM | |
Posts: 5 Rating: (0) |
Hi SteBo, thanks for your reply. I tried your suggestion but it did not help as well. Some other ideas?
|
9/27/2013 11:21 AM | |
Posts: 5 Rating: (0) |
Thanks for all the replies I got it fixed now. It was the server data package missing. Best regards. Downman
|
This contribution was helpful to1 thankful Users |
Follow us on